Other Parts Discussed in Thread: BQ24295, BQ25606, BQ24297
Hi,
I am trying to use the bq24295 as a standalone charge controller for a single-cell 2000 mAh Li-ion battery. Schematic below for reference.
My understanding is that the default charge current for the bq24295 is 1A (based on this thread). I am using a 220 ohm resistor from ILIM to ground, which I believe should be about 2A (although I think that ILIM is input and not charging current?).
In any case, when I try to actually charge my battery I was seeing a charge current of about 450 mA initially (when the battery voltage is quite low, about 3.3 to 3.4 V), dropping to about 100-160 mA after 15 minutes, when the battery voltage was more like 3.5 V or more.
I checked a few hypotheses for what might be causing this:
- Vin is 5.12 V (from a power supply outputting nominal 5V that can provide up to 3A) so I don't think the VINDPM threshold is causing the behavior
- I tried changing the value of the ILIM resistor, and it has no effect on the charging current
- The voltage on the TS pin is 3.01 V and I believe that VLTF = 3.68 V, VHTF = 2.36 V and VTCO = 2.23 V so I don't think it's a temperature issue
Any advice on why the charge current is so low? Thanks very much in advance,
Brian