This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050EVM-561: Why does my BQ40Z50EVM561 can no longer connect to bqstudio via EV2400

Part Number: BQ4050EVM-561
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Hi there,

I used bqstudio to log the charging and discharging data through EV2400 to my BQ40Z50EVM which has a 4S battery cells connected to it. The whole system worked well for around 1.5 months until an unexpected PC reboot(may be windows update) happened yesterday. After the reboot, the bqstudio can no longer hook up to BQ40Z50EVM561 through EV2400, Please help to let me know what can I do! This is the 2nd EVM I have purchased because it failed on the same symptom.

Can I use the sample BQ40Z50RSMR-R2 chip to replace the IC chip on the EVM board, so that the EVM can be hooked up by bqstudio again? or any short cuts are there?

Many Thanks!

Daniel Yu