Other Parts Discussed in Thread: TPS7A30, , TPS54160, TPS62125
Hi,
I have a positive Vin rail, and need to generate a negative Vout for use as a power rail with bipolar supply analog components.
My output needs are:
-10 V > Vout > -16 V (target Vout is -12 V)
Iout >= 150 mA
Low Ripple/Noise
I will be filtering this switching inverter output with an LDO (TPS7A30) for ripple and noise suppression.
My question is how to implement an inverting buck/boost IC in a non-isolated design when using a system-wide ground plane?
Wouldn't the inverting circuit cause greater issues with ground noise than it's non-inverting equivalent?
As the analog circuits are rather sensitive (>120dB dynamic range) is it still okay to simply use a ground plane? Would it be detrimental to attempt to filter the switching noise that will be entering the ground plane?
Or should I simply leave ample distance between the inverter and any sensitive circuitry to minimize ground contamination?
I have tried to find the answer in the many application notes Ti has on inverting buck converters but it seems they mostly describe schematic design and component selection, not potential issues during system integration.
Regards,
Harrison Burch