Part Number: LM25066IA
Other Parts Discussed in Thread: LM25066, PMBUSMGRGUI-SW
Hi All ,
A csutomer at a bringup phase claims the following :
"Using the LM25066IA Hot Swap controller that is following an LM5140 20A/12V buck :
Looks like that the LM25066iA shuts down when we switch on a 20A load.
If we start with a 5A we can go higher to 20A and even up to 25A of Ccurrent limit set point."
When they have tried to use a lab supply and ramp in the same way @ 20A load it seems that our devices gets into an unknown state when it fails to start.
What can be a reason for this inablity to start in front of these 20A (using an electronic load) ?
This thread needs an urgent support
Best regards ,
Arik.P.
AFAE