Other Parts Discussed in Thread: TPS55010
I have just tested the TPS55010 Evalboard. In idle-mode, only supply (5V) connected I measure input current 75 mA.
With 50mA load, I measure input current 128 mA @ Vin=5V. That do not comply with the high efficiency specified in the Evalboard documentation.
The eval board, is direct from the box, no modification. If measure with thermal camera, the heat is generated in the IC.