This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54228: Minimum On Time

Part Number: TPS54228

Hi

My Customer has question.
The customer says it can not be adopted unless the contents of the question clear.
Please give priority to this question and respond.

Customer's spec is as follows.
Vin =6V~17V
Vout=1V
Iout =335mA

If there is a provision of Ton min, please tell me the value of min / typ / max.

The specification of datasheet P5 [tON] is understand to be On time under the test condition of [Vin = 12V / Vout = 1.05V].
In Figure 5, there is a graph of [inputVoltage vs outputVoltage].
This graph means that [Vin = 18 V / Vout = 1.05 V] can be outputted.
However, there is no provision of Ton min in the data sheet.
The customer wants to know if it is possible to output when Vin = 17.5V / Vout = 1 V.

Best Regard
T Kishi