Other Parts Discussed in Thread: BQ24115, , BQ24125, BQ24105, BQ25570
Hello,
I am looking for suggestions to build a charger for a 2.7V lithium ion battery.
This are my specifications.
1 Charger for 1 cell 2.7V lithium ion battery
2 Charge current 240mA or 480mA
3 Stand-Alone Charger
4 Prefer with 5V, 500mA input (USB)
5 Prefer with termination current: 1.2mA
6 Prefer with safety timer
It seems the BQ24610, BQ24105, BQ24115, BQ24125 can adjust the battery voltage down to 2.7V,
but I am not sure whether those ICs are suitable or not.
Any suggestion or recommend suitable device is appreciated.
Thank you for the help