This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ33100: Finding the right part

Part Number: BQ33100

what we’re trying to do is charge/discharge a single UltraCap cell (10, 25, or 50F). We were looking for a bidirectional DC/DC converter IC that will work with a constant output voltage equal to Li-ion battery, somewhere between 3.6 and 4.2V. However we are more than glad to look into two unidirectional components, one path for charge, one path for discharge.

 

We want to discharge UltraCap with max 800mA (at DC/DC output, that is, constant 4.2V), charge with maybe 200mA (again at the constant 4.2V side). We are flexible on charge current and can discuss if it helps. The 800mA discharge current is peak and expected to last 1ms, continuous current in the 300mA range.

 

Components like the BQ33100 seem to have functions (like cell balancing) we don’t need. We definitely overshot with the LTC3110EUF. We are not looking for all that functionality, and pricing has become a significant issue.

  • Hi Laura,

    The bq33100 is a super capacitor pack manager and may be suitable for your application - gauging and management. The device is able to support 2-5 super capacitors in series (or more in stack mode, e.g., no cell balancing).

    This device does not include a bidirectional DC/DC converter for charging. Please check out the EVM for an example circuit with the bq33100 and discrete linear charging scheme. The bq33100 EVM User's Guide may be found here: www.ti.com/.../sluu466.pdf .

    Cell balancing may be disabled with the bq33100, if required.

    Please contact an Application Engineer in the charging forum and/or DC/DC converter forum for charging and/or DC/DC conversion, respectively.

    If you have any other questions with respect to the bq33100, please let me know!

    Sincerely,
    Bryan Kahler