This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6C5712-Q1: PWM Dimming Duty

Part Number: TLC6C5712-Q1


Dear, Sir.

My customer is looking for the LED driver 20mA each output current. They are also expecting

3 different PWM inputs & assigning capabilty refered these 3 PWM's onto each multi-channel

outputs. I believe TLC6C5712-Q1 would be most suitable for such requests.

So, I would like to make sure several things as belows. Please give your advice.

1. PWM Minimum On-time Duty Cycle.

   a) The dtasheet is defined the minimum duty 0.1% or 5us minimum on-time.

       The customer will use 160Hz as PWM input. I wonder 0.08% become as

       minimum duty (5us/6.25ms * 100)?

2. PWM Maximum Off-time Duty Cycle.

   a) The dtasheet is defined the maximum duty 99.2% or 40us minimum off-time.

       The customer will use 160Hz as PWM input. I wonder 99.36% become as

       maximum duty (100-40us/6.25ms * 100)?

Best Regards,

H. Sakai