This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217: TPS65217 AC/USB Issue

Part Number: TPS65217

Dear TI Team.

I have a question about the design of the TPS65217.

1. AC/USB Input

AC / USB is designed to be powered by the same DC adapter.

However, in the design guide, Floating is specified for unused pins.

Can the problem occur when using AC / USB with the same power as below?

Can you tell me why I should not use it together?

2. Question if does not have a battery

If the slva901 document does not have a battery, it will provide instructions on how to design the RLL resistor to GND and how to design the pull-up.
Should I design an RLL resistor?
Float if slva686b is not used.
What if I do not design an RLL resistor?

Thanks.


  • Hi Chun,

    Thank you for your interest.
    Regarding the first question. You are right, the TPS65217 can be powered with a single supply (Vin, DC adapter). It internally decides whether the AC or USB pin level will be routed to the SYS pin. When you only have one supply, then you don’t receive any benefits by connecting the two pins (AC and USB) together. We recommend to connect Vin to AC (or USB) and connect the unused supply pin to GND.

    Regarding your second question. You are correct, as stated in the slva686b you can leave the pins BAT and BAT_SENSE floating. BAT and BAT_SENSE must be connected to each other. If you want to prevent a lockup caused by a brownout on Vin, you can follow the guidelines 3.1 or 3.2 in slva901. To answer your question if you don’t design a RLL resistor you risk a lockup.

    I hope this answers your questions.

    Regards
    Kevin
  • Chun,

    Kevin's advice is correct.

    With no battery, you must still short BAT_SENSE to BAT. TS pin is left floating by itself.

    BAT should be tied to GND through a light load resistor, RLL (1k-10kOhms), to discharge excess energy on this pin when AC is removed and re-applied quickly. If this cannot happen in your application, RLL can be DNP (not populated) and then BAT/BAT_SENSE will be floating.

  • Dear Kevin.

    Thank you for your quick reply.
  • Dear Brian Berner.

    Thank you for your quick reply.