This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR70503: LMR70503 is getting damaged

Part Number: LMR70503


Hi ,

We are using LMR70503 in one of the our design. It is connected to 6 Op amp buffers. We calculated the required current for buffers , it is around 50mA which withing limits of LMR70503. We are seeing in some of the boards LMR70503 is getting damaged [ Not giving expected voltage. It is giving around 0.3V to 0.6V]. Please let me know the reason what could damage LMR70503??

Specifications:

Refer below attached image. 

Input Voltage : 5V

Output voltage : -5V

Required current drawing capability : 60-70mA