This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Help Picking LED Driver

Other Parts Discussed in Thread: LM3410

Which part would you recommend to use for the following:

Drive single LED string with 50-75mA of constant current.

Number of LEDs: 5 to 8 (1.4V per led)

Available Power Supply Voltages 12V (8min 14max) or 3.7V +/-5%.

Dimming is not required, just on or off.

Thanks.