Hello TI,
i stuck with the calculation, when the shim inductor is not needed in the design.
In the design review for 600W PSFB http://www.ti.com/lit/an/slua560c/slua560c.pdf
the equation 120 onwards require me to have a value of shim inductor. If i select the shim inductance to be 0 H, then i get division-by-zero in the equation.
- How should i select the appropriate delay time, to achieve ZVS down to 50% load just like in the design review?
- Should i program the delay time t_ABSET to the minimum value of 30ns?
Thanks