Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hi Guys
I am trying to get theBGQ27750EVM running with the EV2300.
I have installed the Battery Management Studio following the getting started guide.
[Hindsight :
Step 2 did not happen:
'If the Communications Interface Adapter was not previously installed, after the bqStudio installation,
a TI USB DRIVER INSTALLER pops up. Click Yes for the agreement message and follow its instructions.
Two drivers are associated with the EV2300 and an additional file may be required for the EV2400.
Follow the instructions to install both. Do not reboot the computer, even if asked to do so.'
Step 3 neither :
Plug the communications interface adapter into a USB port using the USB cable. The Windows system
may show a prompt that new hardware has been found. When asked, "Can Windows connect to Windows Update
to search for software?", select "No, not this time", and click Next. In the next dialog window, it indicates
"This wizard helps you install software for: TI USB Firmware Updater". Select "Install the software automatically
(Recommended)" and click Next. It is common for the next screen to be the Confirm File Replace screen. Click No
to continue. If this screen does not appear, then go to the next step. After Windows indicates that the installation
was finished, a similar dialog window pops up to install the second driver. Proceed with the same installation preference
as the first one. The second driver is TI USB bq80xx Driver.
]
It did not pick up my device upon start.
I tried to manually select it from the list of supported boards, it wasnt there.
I found the '1750_0_04-bq27750.bqz' file here, in a support request. Tried that, nothing.
I then saw some unknown devices in the windows device manager.
I then figured that perhaps there are drivers missing from the installation (Step 2/3 did not happen, but alas I dont always worry about that, as I am used to SW/docs not being in Sync).
I manually downloaded the drivers and installed them from "https://e2e.ti.com/support/power_management/battery_management/f/180/t/128220"
Step 2 and 3 did not happen. However, the BQStudio worked...I went home.
This morning I came back, and it was no longer working / communicating. Nothing I do can make BQStudio find my connected device. REboot, reinstall etc.
Please help!
Many thanks,
Eugene