Part Number: LM3405A
Other Parts Discussed in Thread: LM3405, LM3406, TPS92515, TPS92511
I am working on an LED retrofit to be used with an AC-dimming Halogen lamp supply. (10,000 units in the field!)
This will be running a single white LED at about 1 A max.
Since this will be running off pulsating DC, I wanted to make the boost supply power up as soon as the source comes up.
The first page "Typical application circuit" assumes a known, constant Vin. So, my plan was to put a 5.1 V Zener between Boost and SW, and feed Boost with a resistor to Vin.
This ran FINE on a bench power supply at 12 V, but when I connected it to the dimmer supply, the LM3405 failed with a short between Boost and SW.
Probably due to a soft knee on the Zener, I'm only getting about 2.8 V from Boost to SW, so may need to feed it more current.
But, can anyone see a real problem with using a Zener between Boost and SW to limit the Boost to SW voltage? Is there any issue with this circuit essentially being powered on and off 120 times a second?
At first I thought Figure 25 was not applicable, as the Vout would be too low with just ONE LED. But, maybe this is a better circuit, although it would run with less Boost voltage.
Thanks for any thoughts and advice!
Jon