This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24720: TPS24720 Storage Temperature

Part Number: TPS24720


Hello,

I'm using the TPS24720RGTT and I see that the operating temperature range is -40C to +125C.  Is the storage temperature range the same, or can it be stored down to a lower temperature?

Thanks,

Steve

  • Steve,

    It is a very good question. There is a reason why it isn't on the DS. Storage temp affects the packaging. There should be documentation that comes with the shipped reels as this is most likely dependent on the IC package itself and plastics material in the reel. I have this into our QA group to see if there is a specific document I can pass to you on E2E but if you have a reel available you might want to look at what came with your device documentation in the meantime. After mounting, obviously it can be stored at the full operation temp range, but not specified to go beyond this range as you might desire.

    Brian