Other Parts Discussed in Thread: UCC27714
Hi all,
My customer want to use UCC256303 for 3kW output use.
Please give me the detail connection cct. between UCC256303 and UCC27714.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Doi-san,
Yes. UCC25630 RVCC can directly connect to UCC27714 VDD.
Please let me know if you have any other questions.
Best regards,
Yalong
Hi all,
My customer tried, but over 2kW, it does not work well, noisy or minus voltage.
This is because 4 x MOSFET use, I think. Two SiC 40mohm is better.
Please let me know the connection such as,
UCC256303 + two UCC5310MC drive-> two 40mohm SiC
My customer have isolated +/- voltage cct. for UCC5310MC outputs.
And my customer want to another plan for Input 700V DC output 4kW 60V.
Is there any method to use UCC256303 with bus voltage 700VDC?
Depletion mode small FET can be used for this case?
If yes, give me the recommended cct.
Thank you.
Hi Doi-san,
1. How to connect UCC256303 to two UCC5310MC. (If you can use non-isolated gate driver, I think that will be ok as well)
Low side:
UCC256303 LO connects to UCC5310MC IN+
UCC256303 GND connects to UCC5310MC GND1
UCC256303 RVCC connects to UCC5310MC Vcc1
UCC5310MC GND1 connects to UCC5310MC Vee2
UCC5310MC Vcc2 connects to UCC5310MC Vcc1
High side:
UCC256303 HO connects to UCC5310MC IN+
UCC256303 HS connects to UCC5310MC GND1
UCC256303 HB connects to UCC5310MC Vcc1
UCC5310MC GND1 connects to UCC5310MC Vee2
UCC5310MC Vcc2 connects to UCC5310MC Vcc1
2. Can UCC256303 used for bus voltage 700VDC?
It is possible but need some extra circuits.
The maximum voltage for HB (HS) is 640V. So HS pin cannot directly connect to the switching node. A high voltage resistor divider can be used to scale the switching node voltage to below 50V.
HB pin cannot be supplied from a bootstrap diode, but instead need to supply from a isolated power supply.
An isolated gate driver is needed as well. Use UCC5310MC as an example, the connection (high side) will be:
UCC256303 HO connects to UCC5310MC IN+
UCC256303 HS connects to UCC5310MC GND1, and also connect to the middle point of a resistor divider from switching node
UCC256303 HB connects to UCC5310MC Vcc1, and also connect to a isolated power supply output
UCC5310MC Vee2 connects to switching node
UCC5310MC Vcc2 connects to another isolated power supply output
Please let me know if you have any further questions.
Best regards,
Yalong
Doi-san,
Let's me check with our designer and I will get back to you.
Best regards,
Yalong
Hi Doi-San,
Sorry for the delayed reply.
1. Pulse Amplitude should be more than ? v .
Suggest to have a resistor divide to make the peak voltage of HS pin between 50V and 100V
2. Maximum Impedance of HS bottom to UCC25603 GND (or low side FET Source).
The leakage current for HS node at dc voltage 160V is 2.5uA, and 4uA for HS node at dc voltage 640V. You can use this to choose the resistor divider values.
Best regards,
Yalong
Doi-san,
It is ok to have the peak voltage between 500V to 600V. In terms of the time delay, you are right that smaller upper resistor will make the delay time smaller. The importance of this will depend on how large the parasitic capacitance is.
However, the reason I suggest to have the peak voltage between 50V to 100V is because slew rate detector for adaptive deadtime control works better for a smaller HS node voltage.
Best regards,
Yalong