This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659039-Q1: Is it same FOOTPRINT?

Part Number: TPS659039-Q1


Hi Support Team,

We are using this PMIC TPS659039-Q1 part in our system. Orderable part no is O9039A385IZWSRQ1.

But the received part is P09039A385IZWSRQ1.

1. Can you help me to differentiate this two part??Is there any change? 

2. Both part are same (Function wise and pin mapping are same)?

3. PCB footprint and pin out are same for both part right? 

4. Can we use pre-production part P09039A385IZWSRQ1 on the place of O9039A385IZWSRQ1?

  • Dhaval,
    There is only one foot print for this part. The pin out is the same. The part number is correct and the OTP setting are the same. The only difference is the P at the beginning, which stands for pre-production material. If this part has been recently released, that would explain why some parts still have the P.

    I am forwarding your question to the product specialist to confirm all of this. He will be able to identify why these parts are labeled with a P.

    Thank you for using E2E.
  • Hi Dhaval,

    Is this the same question as this post from yesterday?
    e2e.ti.com/.../649733

    The answer should be the same - both parts have identical functionality and pinout, so you can use PO9039A385IZWSRQ1 in place of O9039A385IZWSRQ1.

    Regards,
    Karl