Other Parts Discussed in Thread: GPCCHEM, , BQSTUDIO, , EV2400
Hi,
I got new battery with different capacity (1020mAh) for which I'm trying to generate golden file using BQ34z100 fuel gauge. FC bit never set when charging to full.
Used default chemistry in fuel gauge for my battery (Nokia BL-5C). Calibration values used for this learning cycle are generated long back with old battery (2150mAh). I have used bq Gas Gauge Evaluation Software (which I'm comfortable with used for my old battery learning cycle) for this learning cycle. Attached are the latest logs from this GUI.
Some of the Important settings which I changed while running learning cycle are mentioned below:
Taper Current: 150mA (130mA also set in another run)
Minimum Taper Capacity: 25mAh default value (2mAh and 0mAh also tried)
FC Set%: 100% (-1% also tried)
After doing all the above changes also, FC bit never set. Because of this, I was not able to complete my learning cycle after trying for a week.
Pls help what causing the issue.
Thanks
Vidyasagar