This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60150: "Enable" On/OFF at Flashing

Part Number: TPS60150

Hi

My customer has question.

The customer wants to turn ON/OFF the TPS60150 with a signal to turn ON/OFF the LED of the load. (Request specification on the load side)
ON / OFF is scheduled to be performed with a signal of maximum 166 Hz (ON: 6 ms / OFF: 6 ms duty: 50%).


At this time, is there any possibility of problems with TPS 60150?
Is it OK to turn ON / OFF with such a signal?

Best Regard

T Kishi