This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61230A: current more than 20mA with no load

Part Number: TPS61230A
Other Parts Discussed in Thread: BQ21040,

HI

i need your help.

i have a project which use BQ21040 as charger, and TPS61230A as boost, boost to 5V, the power topologies as below. when i test the circuit, i find the current is about 33mA when i input 3.8V(lower than 4V) to TPS61230A directly(just put the TPS61230A and related components, no BQ21040 and TLV1117-3.3, no battery), and when the input voltage is bigger than 4V(the voltage drop between output and input less than 1V), the current meet the datasheet(less than 1mA with no load). i don't know what  happened. i designed the schematic follow the WEBENCH, and layout follow the datasheet.

the output voltage is OK, it is 5V.