This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175-Q1: Webench or LM5175QUICKSTART-CALC

Genius 4840 points
Part Number: LM5175-Q1
Other Parts Discussed in Thread: LM5175QUICKSTART-CALC

Our customer consider to use LM5175-Q1. 

Vin=6V to 18V

Vout=5V

Ioutmax=14A

Fsync=500kHz

Which tool you recommend  they should use Webench or LM5175QUICKSTART-CALC to design?