Other Parts Discussed in Thread: TPS659037
Hi,
In the datasheet of the LM73606 it is written that PGOOD output is low if EN is low and VIN>2V (VPGOOD_VALID, typical 1.3V). If we use BIAS Pin to supply the LM73606, is still the VIN level the criteria to when the PGOOD signal is valid? Or is it: (VIN>2V OR VBIAS>2V)? From the functional block diagram this is hard to tell.
This information is important for us as we need to decide wether we can use PGOOD signal to start/stop TPS659037 PMIC or we need an additional supervisor.
Best regards,
Patrick