This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560200: Duty cycle tweaks

Part Number: TPS560200
Other Parts Discussed in Thread: TLV62585, TPS62821, LM3691,

Hi,

With 4.75V input and 3.3V output (150mA load) the duty cycle seems to cross 70% and this does not seem supported. Down to 4.9V input, the simulation in Webench will be OK, but not lower than that. Can anything be done on the passives on the output that can make us meet our goal?

Please elaborate what device feature is limiting this scenario.

Thanks. /M.A.M