This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60150: PFM/PWM Transition point

Part Number: TPS60150


Hi

My customer has question.


Can you get answers about the following contents?
* It does not matter if content can not be answered when confirmation is difficult.

1.Although the transition threshold of PFM⇒PWM is described as 8 mA (typ), is there a min / max value?

2.When load is increased from 0 mA, PFM ⇒ PWM transits in the vicinity of 8 mA.
 When load is reduced from 20 mA, PWM ⇒ PFM transits around 3 mA.
 Is it correct that the transition point is different?

Best Regard

T Kishi

  • Owing to process tolerance, there 8mA threshold may be slightly higher or lower. Unfortunately I don't have the exact number for the min and max. Regarding your 2nd question, it is because of the hysteresis of the threshold. This prevents the circuit from frequently entering and coming out of the PFM mode when the load is just at the boarderline.