This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54061: Very low load situation

Part Number: TPS54061


Hi,

My customer thinks to using TPS54061 under below situation.
When load is 100uA, Can TPS54061 regulate 3.3Vout?

[Situation]
Vin=24V
Vout=3.3V
Iout=100uA~30mA(Iout max=100mA)

Best regards,
Shimizu