Hello, I designed an isolated DC/DC power supply with LM5017 and have noise and temperature issues. Transformer: LPD8035V-333 Coilcraft
Vin_min=36V
Vin_max=56V
ILoad_sec_max=250mA
Vsec=5V
Attached you can see the signals on feedback node, SW-Node and transformer current on the primary side.
- There is transients on feedback voltage and current I would like to eliminate. Could you give me a hint what could cause this transients and how can I avoid this?
- The transformer surface temperature is 52°C @Vin=56V, ILoad_sec=200mA. Because of small hermetic housing of the application, I would like to achieve max. 40°C. Besides the transformer parasitics, which design parameters affect the transformer temperature also?
Thank You in advance!
Max