This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161: Pre-load resistor in an isolated fly-buck topology

Part Number: LM5161


Hello,

I am designing with LM5161 and for the various calculations I am using your Excel file (LM5161 FBK Quick Start Calculation). The schematics in the file uses a 2 kohm "pre-load" resistor; a note says it is used for regulation at no load, but I am not able to find references about this resistor on the part data sheet.

My design has four identical isolated lines, each consuming about 1.5 W. By using this resistor I have about 240 mW on each line, for a total extra power consumption of about 1 W over a total of 6 W (17% extra power), so it is relevant to the total power budget.

Can you please explain why I should use this resistor?

Thanks in advance.

Best regards,

Stefano Infante

P.S. sorry if this is not the correct forum, but when I select LM5161 as the part number I can only choose this forum...

  • Hello Stefano,

     

    The pre-load resistor ensures that peak charging of the output caps remain minimal.  The 2k is a suggested value.  You can experiment with high value resistors, the performance or load regulation will depend on a number of factors, one more significantly is leakage inductance of the transformer and a no load condition on a particular rail.  If the rail is unloaded, this is when the regulation will be worse and the need for pre-load is more critical to maintain good regulation.  If you always have a load on the rail, then a pre-load resistor will not be needed.

    Hope this helps?

    David.

  • Hi David,

    I have a somewhat constant load, but I also have to provide a way to disable it (by using a solid state relay).

    Hence, when the load is disabled I have no load and then, according to your suggestion, I need a pre-load resistor. But what if I use a double SSR in order to insert the pre-load resistor only when needed? I think I could arrange  a couple of SSRs in order to alternatively enable load or pre-load (see the attachment). What do you think about it? Could the operation of inserting and interrupting the lines generate unwanted pulses which can damage the circuit?

    Thanks,

    Stefano

  • Hello Stefano,

    Understood. what is your regulation requirement? You can implement a pre-load using a Zener diode, in place of a Resistor, that way the Zener only Conducts when its Vz rating is exceeded at the output, without the need to switch anything in?

    Hope this helps?

    David.
  • Hi David, do you mean something like the attached circuit?

    As the transformer output will be about 22 V, I think I could use a 20 V Zener diode with a, say, 2k resistor in series. Do you think this should be ok?

    Thanks again

    Stefano

  • Hello Stefano,

    No need for the Resistor in series with the Zener, the amount of clamping energy is very small at light loads, equal to approximately the energy as a result of the leakage inductance (0.5xI^2xLleak).

    hope this helps?

    David.