This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: When Duty>90%

Part Number: TPS61170

Hi,

Could you tell me about this device?

Can this device be controlled correctly under the following conditions?

【condition】

Vin=3.3,Vout=35.34,Iout=25mA

Although duty is over 90% and exceeds recommended operating range, Webench operates under this condition, so please give us your view.

Best Regards,

Yuto Sakai