This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do you have any RESET IC which can be set 400mV as hysteresis?

Other Parts Discussed in Thread: TPS3808, TLV3011

 Hello guys,

 One of our customers is looking for RESET IC which can meet the following requirments. Could you please tell me any recommended parts number?

 1. RESET detect voltage = 2.1V.

 2. RESET release voltage = 2.5V. (Hysteresis voltage = 0.4V)

 3. RESET release delay time = 60ms.

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.