Other Parts Discussed in Thread: PMP20183
Hi,
I am considering the circuit using the LM3481 device.
The specification is below.
I believe that reference design PMP20183 can be used as it is close to my specifications.
However, the minimum value of VIN of PMP20183 is 9V.
Is the PMP20183 operable with an input voltage of 5V?
(specification)
VIN:5V
VOUT:100V to 200V
IOUT:10mA
Best Regards,