Hi expert,
We refer to two different documents that they all mentioned the intervals to get the CC value.
1. In "tiduar8b.pdf" chapter 4.2.6 - Firmware, ....ISENSE (battery current through the shunt resistor) is checked with a 10-ms task loop,
2. In "bq76940.pdf" chapter 7.3.1.1.3 - 16-Bit CC, A 16-bit integrating ADC, .......... The integration period for this reading is 250 ms.
They are both using BQ76930 AFE, why the intervals are different and which one should I use?
thanks