Other Parts Discussed in Thread: BQ40Z50-R1
Hi all,
I'm testing a new circuit with BQ40Z50-R2.
I can communicate freely with a different board with BQ40Z50-R1 on it with the exact same schematics (but different components arrangement).
I can see the SMBUS signal on the scope and everything is fine.
when I connect to the new board I made with BQ40Z50-R2, I see a flat 0.7V on both lines.
so far I tested:
1) correct voltage on all cell pins, BAT and VCC are powered.
2) SMBD and SMBC are reaching the IC pins in a good manner.
3) shorted the PACK+ and BAT+ as EVM circuit suggests to start the IC action.
4) when nothing is connected to the EV2300, I can see the voltage on its SMBUS data line of 3.3V trying to write and waiting for answer.
this means that it is pulled down to 0.7 as soon as connected to the board.
what can be the reason?
what can I test to understand this issue?
best regards, Ran