Other Parts Discussed in Thread: LM3410, , LM36010, TPS61160, TPS61165
Good evening to everyone,
I would like to know if is possible to use the TPS61160A in SEPIC configuration like, for example, the LM3410 can do.
I prefer TPS61160A agains LM3410 because it offer an "analog dimming" for led current and also the embedded open led condition.
My power is from a LiPo battery that can start from 4.2V and can go down to 3V and i've only 1 led at the output with 800mA with maximum current and almost 3.7V for forward voltage.
Regards, Luca