Other Parts Discussed in Thread: LM5176
Tool/software: WEBENCH® Design Tools
Hi Team,
I'm developing lead battery and supercapacitor charging device based on LM5175.
10-16V IN ….. 0-15V 6A OUT
To make preliminary calculation I use WEBENCH® Designer LM5175.
CCM - mode; DITHERING - disable; aux. BIAS supply - 10V; Frequency 100 KHz;
Overcurrent Protection 5mOhm; Output Current Limiting 6mOhm;
If I connect resistive load (lamp or resistor) - the device works correctly in all modes.
Efficiency 92-97% and minimum power dissipation of all active components - they are a little bit warm.
But if I connect discharged lead battery 12V 60AH or discharged supercapacitor 300F 16.8V the device is working, but power dissipation of transistor HDRV2 and DIODE in BUST SIDE becomes 10 times more! (VD8 and VT3 in my schematic )
As a result - transistor and diode are incredible HOT! After 15 seconds I have turn off the device - otherwise the diode will be destroyed! I see this effect in all 3 modes buck, bust and buck-bust. My schematic is attached.
Can you help me to arrange this problem?
Thanks!