Tool/software: WEBENCH® Design Tools
Hello
I am using the TPS63070 for the first time in a battery powered application. I followed the following web bench design. The design is for a output voltage of 3.3V from a single cell Lithium Ion battery. But the results are drastically different. The output voltage I get is over 10V and the voltage on the feedback pin is over 2V. How can I trouble shoot this?
PG pin is always low. Essentially the regulation does not seem to be happening.
I have tried 1uH and 2.2uH with 20uF and 47uF output capacitors respectively. Under no load and light load conditions.
I have used many web bench designs in the past with reliable results everytime. This is the first time I am having a problem with a web bench design.