↑:Based on this thread, I set up a new thread.
When generating a negative voltage circuit, I will assume the following circuit diagram.
<Specification>
VIN: 20 to 36.6 V
VOUT: -12 V
IOUT: 0.3 A
Can you tell me the setting values of peripheral parts when designing with this specification?
(Please correct even if there is an error in the circuit diagram.)
Best regards,
Masumi Sekiguchi