Hi team,
I'd like to ask about BQ25570 threshold temperature of thermal shutdown.
The thermal shutdown is described in D/S 7.4.4, but the threshold temperature is not defined.
I think this device threshold temperature is min 85 deg, because the D/S is mentioned max temperature is 85 deg in "Recommended Operating Conditions".
In short, if the ambient temperature is until 85 deg, it must be work.
Is my understanding correct?
Best regards.
Hayashi