Other Parts Discussed in Thread: UCC28630, UCC24630, UCC24650
I'm trying to design a high voltage (~2kV) isolated capacitor charger based around the UCC28633 controller. I have chosen this device due to the PSR, good documentation, and apparent constant current limiting.
I am having trouble predicting how a circuit would behave in constant current mode for a sustained period of time. The primary would receive a signal stating that the desired voltage is reached via an optocoupler. I need this signal to immediately disable the charging.
A potential issue occurs if at low voltages. If the circuit feedback is designed for a constant voltage output of 2000V, but the external over-voltage circuit is set for 100V, the issue would occur. If running at constant current, when a capacitor reaches 100V, the output power of the PSU is a small fraction of the nominal power, and therefore I would expect the controller to be in low power mode. Therefore, the shutdown pin (Pin 2, for an NTC) is disabled, and I would have no way of turning off the output.
I think this wont be an issue, due to the full current flowing at the output, and therefore, large reflected currents occurring at the input. This would mean that the internal modulator is actually running at a higher demand level, and therefore, pin SD is still enabled.
My question is, am I correct? Does anyone have any advice they can offer on using this part, or recommendations for different converter topographies/controllers.
I realize this is a very open-ended question, but any assistance is greatly appreciated. Let me know if there's anything I can add in explaining what I am trying to do.
References: SLUSBW3C, SLIC015C, SLUC537D