Hello, I am developing MPPT circuit in which I don't need to charge the battery. My need is constant output voltage around 12V which drives the load directly, I refer BQ24650 reference design. Bq24650 try to detect the battery presence at the output. Does it is possible to connect the load directly to BQ24650 without using any battery? Can we stop the battery detection in BQ24650? Thanks.