Part Number: TPS7A85A
Other Parts Discussed in Thread: TPS7A85
Hi
My Customer has question.
Can you tell me the thermal resistance between "junction TJ" and "ambient temperature TA" at forced air cooling 1 m / s?
Assuming worst case, load current 3.9 A, voltage difference 0.326 V, ambient temperature 75 ° C., forced air cooling 1 m/s.
I want to check if it can operate under this condition.
I think that it is difficult to deal with, but I want comments.
Best Regard
T Kishi