This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751: Class 4 Flyback Converter (24V/1.25A)

Part Number: TPS23751
Other Parts Discussed in Thread: TPS23752

Hello,

I would like to design a PoE PD with the following specifications using TPS23751.

・Vin(min)     36V
・Vin(max)    57V
・Vout(Nom)   24V
・Iout(max)          1.25A
・Class 4    
・Output Power   30W
・Isolated
・Input Type   DC
・Topology   Flyback Converter

Is there any 24V output reference design?

What is the recommended product of 24V output flyback transformer for TPS23751?

For example,POE300F-24L(Coilcraft)?

Best regards,
Seishin