Hi expert,
I have a cell balancing questions about TIDA-00449 implementing.
In the chapter "4.2.6.3.3 How is it Implemented in the TIDA-00449"
There are two check points when to do cell balancing
• At the end of charge when the cells reach 4 V or higher
• When the pack is in idle for longer than 30 minutes and the cell voltage is higher than 3.3 V
Q: We can not find the below check points in simple_charging_balancing() and simple_idle_balancing().
Do you suggest to implement it?
thanks