Part Number: BQ77PL900
We are using BQ77PL900 for 7 cell Li-Ion battery management but facing some issues of cell balancing in standalone mode.
Configuration Settings are as follows:
No of Series cells – 7 Nos
Over voltage Detection – 4.25V (Same as balancing start voltage as per datasheet)
Over voltage Hysteresis – 0.1V
Under Voltage Detection – 2.5V
Under voltage Hysteresis – 0.4mV
External current path (FETs and 56 Ohm resistor) with 10K series resistor used for balancing
Observations while Charging the Battery Pack in Standalone mode-
- When one of the cell reaches to 4.25V (OV threshold), CHG FET is turned OFF.
- Balancing gets start as per the internal algorithm.
- Balancing are observed on all cells (Even on cells which has not reached to OV threshold),
“SET by SET” as per the algorithm described in document SLUA463.
- Balancing does not end on certain cell even if cell voltage drops to recovery voltage level 4.15V (4.25-0.1, OVth-Hys). It is still going on till last cell voltage in that Balancing SET drops to 4.15V. Result is, further voltage drop on the cell which has already reached to 4.15V.
- It happens in all Balancing SETs.
- At the end of balancing, got different voltage readings (Min 4.11, Max 4.15) on all cells in the battery pack. There is 40mV difference observed on different cells.
- CHG FET is turned ON at the end of balancing process.
We need to know:
- Are above observations matches with the functionality of BQ77PL900?
- What is tolerance voltage limits of balanced cells? Which is not specified in datasheet. (40mV in above observations)