This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82150: Generating a negative 5V from negative 15V

Part Number: TPS82150


I was planning to use two TPS82150 devices to generate +/-5V from +/-15V, and have been looking for an application note to generate negative 5V from my negative 15V rail.

I have seen the example Inverting Power Supply Schematic in Figure 30, but this doesn't work for me as +15V to -5V exceeds maximum supply voltage, and it is preferred that I use the -15V rail.

I just wondered if I was missing a simple solution?