This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3481: frequency is not settable or changeable

Part Number: LM3481


Tool/software: WEBENCH® Design Tools

hi, using web bench for my sepic design, which is nice, but the frequency is not settable or changeable.

if I use advanced options, it only allows +-5%.  not a stoppable problem.  but it "crashes", won't work with the advanced frequency option.

also, when I change BOM inductor and inductance values, I expect the frequency to change accordingly, but it remains fixed at 507khz.

what to do?

  • Hi Vern,

    Thanks for reaching out to us for your question.

    I was able to adjust the frequency by checking the user preferred frequency box. Nothing crashed either. Please make sure that your internet browser if up to date.

    The switching frequency is taken as a design parameter. Since switching frequency is considered a fixed parameter it will not change when the inductance value is changed.

    Thanks,

    Garrett