Other Parts Discussed in Thread: LMR14050
Hi team,
My customer want to use LMR14050-Q1 in a automotive panel with local dimming function, in this project, the LMR14050 is used as power supply for LED and LED driver have a control pin connect to LMR14050 FB pin with a resistor in series. LED driver internal DAC would control the voltage on the control, thus changing LMR14050 output voltage.
in this project, customer need to change LED driving current from 120mA to 190mA, thus the LMR14050 output voltage is rised from 5.4V to 8.7V, customer want to know how long time does LMR14050 take to settle the output voltage. a general order of magnitudes should be enough, like less than 10ms/1ms/100us/10us/1us/100ns, etc..
thanks.
Kevin