Other Parts Discussed in Thread: TPS63070,
Hello,
I would like to use the BQ34110 to drive an enable line for a downstream power supply, such as the TPS63070. The enable line should deassert when the battery is below a voltage or power threshold. Driving ALERT1 with either BATLOW or SOCLOW states appear like good choices and I have observed ALERT1 making the proper transition when the battery is discharged below the BATLOW/SOCLOW set threshold. I do not, however, see the return transition when the battery is charged above the BATLOW/SOCLOW clear threshold.
The technical reference manual states, "The Alert1_0..6 Config and Alert2_0..6 Config signals are cleared upon a read of ALERT1STATUS() or ALERT2STATUS(), respectively." Is this the only technique for clearing the state of the alert line? I would like the BQ34110 to control the alert line completely by itself, toggling the enable on and off based on set and clear thresholds, rather than a downstream host processor which could be powered down and unable to query ALERT1STATUS(). Please advise.
Happy New Year,
Christopher