hi sir:
We have question about LNB current limit. we base on datesheet to calculation the current limit. Currently, our l_set resistor is 287K with I_ocp 0.48A.
But this current protection point are different, when 22KHz-Tone enable and disable.
Our verify result as below table
22KHz-Tone
Vout Disable Enable
13.4V OCP = 0.46A OCP = 0.39A
18.2V OCP = 0.46A OCP = 0.39A
When the 22KHz-Tone is enable, the current protection point seem don’t meet calculate formula.
We also verify the TPS65235 EVM and happen the same phenomenon.
The project request is "must be meet output current 400mA."(even if the 22KHz-Tone is enable.)\