Part Number: BQ25895
Other Parts Discussed in Thread: BQ25898D, BQ25890H, TUSB422
Hi,
BQ25895 is adopted for powerbank.
In evaluation with general USB charger, charge current is about 1.67A.
BQ25895 ILIM resistor is set to 2A and charger is connected as DCP as below.
therefore, IINLIM is 3.25A but measured charge current is about 1.67A.
Is it limited by USB charger? USB charger supports 5V, 9V, 12V, 3A and QC3.0.
How can BQ25895 get 12V, 3A from this charger?
Could you check below register set?
Thanks.